This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq500211EVM-045

Does anyone know if this development kit (bq500211EVM-045) can be ordered?  I want to order the bq51013AEVM-765 and bq500211EVM-045 to use in a low voltage system.  My input voltage is from primary lithium batteries (3.6 or 7.2 volts), and I want to regulate the secondary at about 3.0 volts.  Are these the best kits for this?  BTW, I need to be able to evaluate these kits with custom 0.75" coils (~10uH) for both primary and secondary.  Thanks for any comments.

  • Good talking to you today Steve.  I think we resolved the questions.

     Key point about the bq500211EVM-045 TX and also the bq500410AEVM-085 both units are in high demand and we are restricting sampling of the EVM to provide enough coverage of all key customers.  The EVM product folder has a request button which will take the user to an online form.  After the form is submitted it is reviewed by the project and regional sales managers for approval.

    The bq500210EVM-689 is available in the TI eStore with no restrictions.