Hi,
I am using a 30V N-Channel Power MOSFET, CSD17312Q5, in a power management converter. Knowing the current through the MOSFET, I tried to measure the VDS across the MOSFET during ON state through the oscilloscope. Datasheet says RDs(ON) is 1.2mohm for a VGS of 8V. Current through the MOSFET is 10A . Hence VDS across MOSFET should be 12mV. But I am observing it to be around 80mV. I am clueless why the MOSFET is showing around 8mohm RDs(ON). Such a high RDs(ON) is impairing the converter efficiency severly. Any ideas/suggestions?
Regards,
Sutej Reddy.