This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Simulation of TPS27081A high side load switch



Hi,

is there any spice model for the TPS27081 available?

I would like to include it in my global simulation.

The application is an active current limiter between a high impedance source and the large bypass capacitor of a switching regulator. Other current limiters are unsuitable, because I need an adjustable (among different products) solution in the range of about 1mA to about 50mA. Also, quiescent currents are of paramount importance, so I would like to plot the tradeoff between R1 and the leakage current.

Thanks.

 Roberto