Other Parts Discussed in Thread: UCC28070, UCC28070EVM, UCC3817, UCC27322, UCC37322, UCC28019
We are in process of designing PFC with UCC28070 integrated circuit. Power is 400W, 85-265 input voltage, 400V output, 130 kHz. We use TI excel design tool calculator to calculate components values. Problem is when we use calculated components in our design the inductor are very very noisy, operation switches from continuously to discontinuously mode every few pulses (gate pulses are missing) when it should be permanently in continuously mode. Transition from discontinuously to continuously mode is sharp instead smooth one. When we change all components to values as in 300W, 200 kHz, UCC28070EVM evaluation module, operation improves significantly, only sharp transition remains. We check and double check our calculations for mistakes, none found. What can be wrong in our 400W PFC, is 130 kHz to low? Why so sharp transition, when we check transitions on evaluation module board transitions are smooth. Where can we get more informations about cores used in current transformer and inductor in EVM design? Does anyone have more experiences with UCC28070 beside reference design, on web I found only announcements, no practical experiences.