Hi,
I'm looking for a buck converter that is capable off sinking and sourcing.
The output needs to be adjustable so the controller needs preferable an external reference.
Input: 10V -> 14V
Output: 1V -> 5V
Current Source: 10A
Current Sink: 10A
I found the TPS54620 but the sinking limit is set to 2.3A. and still has an internal reference.
or the TPS40056 but this one doesnt limit the low side fet on time.
Any tips on a potential part number would be great.