How is the calibration profile affected if two single cells are connected in parallel to the battery pack instead of a single cell?
BQ27500
Calibration:
- Documentation states that calibration should be done on the host system. How much accuracy error is introduced if calibration is done on the EVM instead?
Production programming:
- The main board does not have access to the I2C lines so will have to use FlashStream.exe application to generate dffs file. Where can I find it?
- Do I need to download firmware+dataflash constants (bqfs file) or just the dataflash constants (dffs file)?
BQ27541
- Can this IC be used for system side implementation?
- Would like to have interrupts for battery insertion/low/good like BQ27500, but this IC does not have those. Read about HDQ interrupt functionality but is it available simultaneously with I2C? If not, looks like Flags() command can give state of charge warnings but are there any status registers that provide battery inserted?