This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2596 battery charger output blocking diode

Other Parts Discussed in Thread: LM2596

I made some further measurements on another LM2596 converter module and it seems to me that there is a built-in diode from output (anode) to input (cathode) inside  the LM2596 chip. This would explain the large current from connected battery at the output to a  zero impedance input connection which blew up the LM2596 chip and the catch diode. A diode from output to input  is not shown on the block diagram in the LM2596 datasheet. Could you please comment on my observation ?

Thank you in advance.