I will be using LM20134 to provide few voltages in my design (couple of core voltages and IO for several FPGAs), and wanted to run inductor choice by you to see if there are any issues.
The datasheet recommends using Coilcraft MSS series inductors (shielded, ferrite core). I was wondering if the XFL4012 series (shielded, composite core) would be ok? Likely XFL4012-601ME, 0.6uH, max DCR 19.14mΩ (http://www.coilcraft.com/xfl4012.cfm). Program is very much size constrained, which is why I’m looking at a smaller footprint.
My Vin is 3.3V, the outputs are 1.0V, 1.2V and 1.8V. Temp range up to 85°C
For current
1.0V at room temperature will be about 1.2A, at 85°C about 3.4A
1.2V at room temperature will be about 0.5A, at 85°C about 1A
1.8V at room temperature will be about 1A, at 85°C about 2A
I don’t intend to use the same inductor for all three, unless it happens to work.
thanks so much !