Hello,
I'm having some trouble with a tps2113a. I've connected it as shown in Figure 14 in the datasheet.
IN2 is not connected at the moment, but IN1 is connected to 4.9V.
With my setup the switch should let IN1 go through.
I checked that VSNS is above 0.8V also even though this shouldn't have anything to say.
Stat should have been 0V, but is ~0.6V ??
and OUT is ~1.6V.
The load is a TPS63001 supplying the PCB.
Daniel