This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2231 – How much is maximum power consumption in the following condition

Guru 21045 points

A customer wants to know the maximum power consumption in the following condition.

 

【Condition】

3.3V Line: Vin=3.3V , Vout=3.3V , Iout=230mA

1.5V Line: Vin=1.5V , Load = Open

AUX Line: Vin= 3.3V , Load = Open

/SHDN = High

/STBY = High

/CP = Low

 

【My guess 】

3.3V Line:PD = R*I^2=68mohm * (230mA)^2=3.5972mW

AUX Line: PD = R*I^2=200mohm * (150uA)^2 = about 0mW

1.5V Line: PD = R*I^2=70mohm * (10uA)^2 = about 0mW

So maximum power consumption is about 3.6 mW.

 

< Parameter >

R = detasheet P3 Power switch resistance at Tj=100℃ (worst case)

I = detasheet P4 Operation input quiescent current at MAX (worst case)