This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40400 abs max rating on HDRV pin

Other Parts Discussed in Thread: TPS40400, CSD86330Q3D

Dear Forum,

I have designed and built a 5.0V in to 1.0V out DC-DC converter using the TI TPS40400. I am using the TI CSD86330Q3D to provide both the high and low switching FETs. I observe that, during the dead time whilst both FETs are switched off (approximately 40ns), the SW switching node falls to -800mV with a brief initial pulse of -1280mV for 5ns. This is as I would expect, due to the dead time current having to flow through the source-drain diode in the low side FET. As stated in the datasheet, the absolute maximum rating on the SW pin extends down to -5V, so this is fine.

However, I also observe that the HDRV pin (the gate driver for the high side FET) follows the SW pin down to -800mV for the 40ns dead time including the -1280mV pulse for 5ns. The datasheet states that the absolute maximum rating for this pin only extends down to -300mV. Is the observed behaviour acceptable, or might this damage the TPS40400 device?

Thanks for your help.

Gavin Jones.