We designed a new project using the LM25085A regulator (as you can see in the image) using the Webench Designer.We designed a circuit with a input voltage range between 22.5V and 25.5V, output of 12V and a maximum current of 5A at the 12V output. We created the schematics and pcb following the results of the webench. We are testing the circuit and it is only able to provide 12V without any load. If we attach a small load (10k resistor) at the output the voltage drops to 1V.
Does anyone here have a similar problem with this CI?