Hi..,
for one of ours USB HUB solution, we are trying evaluate the Power switches. I have basic doubt regarding this.
from my knowledge, USB2.0 allows a peripheral to consume max of 500mA . correct me if i am wrong.
Most of the switches like TPS2041A... states continuous allowed current is 500mA which is compliant to USB2.0.,
But the electrical characterstics says Current limit will be min = 0.67A, Typ = 0.85A and Max =1.01A. what are the conditions for these 3 ratings. if it alows 1A current to pass through without issing Over Current, this is violating USB2.0...