I have found LP3950 LED Driver. This can be done by 1pin-Connect function in Default Mode with Audio Synchronization. But It is not clear, which are default values used in the default mode. In Table 9, it is not apparent.
Is it possible at the LP3950 permanently save commands even after power off und power On?
What values AGC gain, SPEED, MODE_CTRL be used in audio sync default mode?
Are there any other audio sync IC with 1 adjustable PIN Default Mode available from TI ?
Can LP3950 be operated without BOST modules like? With +5 V or +12 V
Where can I find FotPrint Library for EAGLE 6.0 or ORCAD of LP3950?
Is there an easy cheap controller where of a button can send I2C commands to the LP3950.
Is there any way as 8 different colors with the LP3950 to shew, and with fading effect simultaneously. I mean that when you turn off and On the led slowly 10 - to 50 sec go from 0% to 100% light intensity.
Thank you (Sorry for Google translate)