Hello,
I have the MSP430F5529 and bq76PL536EVM-3 modules and i'm trying to verify the cell balancing algorithm with 6 li-ion cells that are connected to the first battery connector as single operation ("Circuit 1" on the EVM). I compiled and downloaded the code provided following the guidelines on Application Report SLAA478, then made the power and communication connections between the MSP430 target board and bq76PL536EVM-3. I can see the SPI signals generated by bq76PL536EVM-3 on my oscilloscope, however cell-balancing doesn't work.
The system works normally when i use bq76PL536 Evaluation software v2.2 in stand-alone mode. What I need is to be able to accomplish cell-balancing without a computer.
Thank you.