hi Bill,
I have a BQ500211 transmitter and it works well. Now,i want to change the BQ500211 replace into BQ500211A, but the transmitter works not well.
i know the 211 and 211A is pin to pin , also i add a resistor connected between LOSS_THR (pin43) and GND ,and then put my phone NOKIA 920(or LG NEXUS4) on the transmitter,at first charge ok, after about 5s .the transmitter red LED fast blink keep about 10s,the BUZ works once time,and red LED keep light--i am sure this mean is PMOD/FOD warning.
At the beginning , I thought that maybe the LOSS_THR resistor value is too small,so i change the value from 42.2K to 200K, but the problem is same. if i Take away the LOSS_THR (pin43) resistor ,leave this pin open , the transmitter works well.
maybe the LMV931 and INA199A have Some of the differences,but i measured the voltage of I_SENSE ,the value about the same.
alse maybe some anyother circuit need to adjust,
so Bill, i need your help,, thanks !!