This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq26200

Other Parts Discussed in Thread: BQ2019, BQ26200

Dear sir

i am working on Bq2019 and want to replace it with the BQ-26200 can you tell how to calculate the value of Rom and Ram file?

Regards

Tanvi Verma

  • Hello Tanvi,

    From the data sheets for both devices, the RAM,FLASH and ID ROM for the bq2019 and bq26200 appear to be identical.

    Page 10 of the bq26200 datasheet provides the memory map for the device.  The memory map for the bq2019 can be found on page 11. You can look at them and verify the locations and size.

    Thanks,

  • Dear Greenja

    Thnx for reply in both datasheets their is no information regarding how to calculate the values of the register i.e if i want to add the value of 0X40-0x5f then how to calculate its value?

    Regards

    Tanvi Verma

  • Hello,

    I'm not quite sure just exactly what you are trying to do or what you are asking.

    Are you asking how to use the commands to read data from the flash register then in your code do some calculations on them?  Or are you trying to figure out what the values mean when you read them?

    Since I'm not clear on your question, I suggest you look at page  13 for the bq2019.  You can see how the data is transfered LSB first.  The commands are listed on the next page. A read of the location would have a 0 in the MSB.

    Hope that helps.