Hi,
I am testing a board using a TPS63002 to generate 5V with a very low load (8mA) and the converter is pulling 42mA at a 4.8V input however based on the datasheet efficiency graph I should be seeing far greater efficiency of about 70%.
I have attached the relevant schematic and layout sections. When I first received the board there were significant stability problems, and the converter would frequently draw several hundred mA and fail to start properly, this instability seems to have been fixed by removing C20 and remounting it immediately to the left of the IC, connected to the power pad on one end and the output trace (with the mask scraped off) on the other. I have also added a 100uF electrolytic smoothing capacitor elsewhere on the board. However both of these had little to no effect on the supply current issue and has not worked on a second board I have modified, so any suggestions are much appreciated.
Is there any guidance for how to select components to reduce the supply current or are there values I should change? The application sees a roughly 5mA load with occasional spikes to 150mA max for several seconds. Is the layout likely to be the cause and is there any modification I can do to the prototype to confirm this?
Thanks.