Hello
This is a very specific question regarding the DGN package for the 3707. Does the PowerPad under the part connect to the GND signal of the part or what signal is the PowerPad connected to?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
This is a very specific question regarding the DGN package for the 3707. Does the PowerPad under the part connect to the GND signal of the part or what signal is the PowerPad connected to?
On the board, the thermal pad can be soldered to a floating plane of copper or to a ground plane. If you connect the thermal pad to ground, you will still need to connect the ground pin of the IC to the board ground. The substrate silicon (ground) of the IC is glued to the thermal pad but this makes a poor electrical connection.
Scott
Thank you very much for the quick response. So the pad than is just needed for thermal reasons. If I wanna use this to replace a MAX708 part which is laid out on a board without the thermal pad than the reprocussions are decreased thermal efficiency right? It seems though the part only draws in the uA range for IDD so I don't see how there could be many thermal issues.
Thanks again,
Gary
Yes. It is not a requirement to connect the thermal pad to anything on the TPS3707. The device normally dissipates a couple of milliwatts which doesn't amount to much thermally.