This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2394 different current ramps

Other Parts Discussed in Thread: TPS2394

Hello,

I’ve got TPS2394 in my design whose behavior is different to evalboard.

They have also slightly different labels:

on Eval-Board: TPS2394 05KG4 D5LO

In Design: TPS2394 23K04 ALLR.

 

I’ve changed evalboard for design tests: Q1=AOB260L, C6 (flt timer)=4.7µF and C7 (ramp==1µF), Rsense=4mOhm.  The load is 47000µF and 25 Ohm in parallel.

 

The problem is that the hot swap controller in the design has some turn on delay and a different current ramp that is more adverse for my MOSFET. I cant measure that behaviour on evalboard.

 

Do you have any idea what is wrong in the design? Was TPS2394 changed?

 

Best Regards.

 

Vitali