Hi,
I need to select a buck converter
Input = 24V +/- 5% tolerance
Output= 5V, 600mA maximum,
I was thinking of using TPS5405 , but going through the datasheet i find there is a pulse skipping mode with threshold around 300mA
my output current requirement may reach that boundary some times...
My product requires a CE certification and needs to pass conducted emission tests...
I was wondering whether it is perfectly ok to select this part..
Any comments/suggestions will be greatly appreciated..
Regards
stephen