Dear all,
we used TPS61176 in our design to drive the LCD, TPS61176 is designed to generate 26.4V and ISET pin is set for 20mA. But at the output SW pin we are getting only 3.69V, we are applying input of 3.8V.
LCD backlight comes up for few seconds when PWM/EN pin is high, after few seconds LCD turning off that time PWR/EN pin goes low.
Also wepulled to high directly to the PWR/EN and tried but only one flicker comes when it boots. We are doubting that, IC going to shutdown mode. Anybody faced this problem ?
In PWR/EN pin is this mandatory to apply PWM signal only because we tried with pulling it to high as well.
These are all the following voltages at all the pins of TPS61176.
Pin1 | PWM/EN | 0 |
Pin2 | VLDO | 3.3 |
Pin3 | ISET | 1.1 |
Pin4 | COMP | 0 |
Pin5,pin6 | IFB6,IFB5 | 1.12 |
Pin7,Pin9 | IFB4,IFB3 | 0.9 |
Pin10,Pin11 | IFB2,IFB1 | 0.8 |
Pin12 | OVP | 0.28 |
pin8,pin13 | GND | 0 |
Pin14,Pin15 | SW,VIN | 3.69 |
Can anybody help us where we are going wrong ?
Thanks & Regards,
Deebak chandar T