Hello,
a the moment I'm trying to verify a power transfer between two boards with the ICs mentioned above. The designed receiver works fine with the purchased bq500211AEVM. But if I put the receiver on the self designed Transmitter board (the low-cost schematic of the datasheet was used as a template), the LED on the receiver which should indicate a charging is not glowing. The transmitter seems to detect the receiver correctly. When I place the receiver on it, the LED connected to BUZ_DC is on for a about half a second or something.
Do you have any suggestions how to detect the problem? When exactly is the BUZ_DC triggerd? Just after detecting a receiver coil or after the successful identification of a receiver with communication packages? In the datasheet it says: "outputs a pulse when charging begins".
Kind Regars
Manuel