I have a new application which I do plan to use two LMZ22003’s. Is it possible to trim up/down the output by driving the FB pin externally using a 0-3V through a resistor? I think it depends on the internal reference voltage. Attached document shows the way I achieved this before. The internal reference has a 1k resistor in series with it and one can use it as a summing junction to modify the reference voltage hence trim up/down the output. I am hoping I can do the same with the LMZ device. Please advise.