Hi All,
The TPS55065 switch-mode regulator does not start at V(driver) less than 5 V.
Once it started it can regulate 5V with input down to 1.5V
Unfortunatelly it is not an option for buck-boost requlator, because it can not able to start with 3V.
Is there an another part that can start with 3V input ?
Best regards.
Note: I have checked TPIC74100 and same situation valid for it.