I have this circuit built, but i'm getting a result that is not expected.
No Load:
Vin = 48V
Vcc = 7.4V
Vout = 6.8V
UVLO = 4.72V
With no load, i get 6.68V on the output, but when i put any load on it, the voltage drops considerably.
with a 47R resistor across the output, I am only getting a 1.8V. The circuit is based on a Webbench design.
Under no load I am measuring 7.4V on the VCC pin
When i probe the SW and FB pins i'm not seeing any ripple at all, its almsot like the thing is'nt switching..
If i stick a 47R/5W resistor across the output Vpout dropps to 1.7V or so...
I've swapped the IC in case i had a faulty one.
Kind Regards
Andrew.