This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3481 and LMV431 Circuit question

Other Parts Discussed in Thread: LMV431, LM3481

Alan, All,

Note the LMV431 here in your circuit, that device is a zener 3 pin not a five pin op-amp as shown here correct, I'm confused?. I have implimented a similair circuit using the LM3481 as suggested and my own op-amp to the FB pin, but the drop across the 100K to the FB pin is so large that the input inpedence of the FB seems to be about 50K is that what you would expect? The way the circuit is drawn it seems the input impedence would be much greater not to lose a large voltage drop before getting to the FB pin. Can you advise?