For these questions assume I'm using the bq27531EVM (bq27531-G1 & bq24192), using a new 10Ah battery (and Design Capacity set to 10000) at room temperature, and my power source provides 17V @ 10A.
1) How does the SOH affect the way the battery is charged? I have read the section "3.2.4 Multi-Level Charging Algorithm" in the bq27531-G1 TRM but it doesn't go into details about it. Is it linear so that when the SOH reaches say 85% then the charge current is overall reduced by ~15% and the charging voltage is raised by ~15%? How much of an effect does the SOH play on the charging algorithm?
2) I am assuming that since the default Charge_Current values at room temp are 100 that the charge current would be limited to 4.5A since 1C of 10000 mA is higher than the 4.5A limit of the bq24192. Is that correct?
3) Is it also correct to assume that it would be useless to program the Charge_Current values to anything above 45 in this case? That way in theory the charge current is limited to the same 4.5A.
4) Say that I was using Charge_Current values of 45 (normally a 4.5A charge current, right?) but the SOH of the battery was 85%. Would it take ~15% longer to charge the battery because the bq27531 is compensating for the lower SOH?
5) I see the Charge_Current settings are based on the C value of the pack. Is the C value used in the charging algorithms just read from the Design Capacity?