Can we get the LP8900, for Vout1=3.3V and Vout2=2.5V or with two adjustable output ?
According to the d/s Output Voltage from 1.2V to 3.6V,but in its ordering information no option for above 2.8V.
Am I missing somthing?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
LP8900 - Dual 200mA Linear Regulator
" ... no option for above 2.8V..."
No, you are not missing anything.
Contacting your local sales representative would be needed in order to determine pricing based on needed production ramp date and volumes.
There a few other options. Check the following to see if it might meet your needs ...
TPS71334 - Dual 250mA UltraLow Noise, Low-Dropout Linear Regulator
Vout1=3. 3V, and Vout2= Adjustable
http://www.ti.com/product/tps71334