I have a customer asking:
- Is there a problem applying the 5V on Vout w/o Vin? During the programming of the board we may need to apply external power to the board rather than using high input voltage.
- The internal current limit of the part is quite high (3.25 A typical)? Can it be reduced with external components (like Ramp generator)? (Thoughts behind question #2: LM5005 is capable of delivering up to 2.5A. In our design we really don’t need more than 1.5A. Since part current limit is high, it seems we need to oversize inductor and Schottky diode to handle overcurrent conditions (that are below LM5005 current limit). Lowering the internal current limit should help.)