I'm designing a power supply with the LM2674;
Vin=12 V
Vout=5 V
Iout=100 mA
I'll be using the 5 V fixed output version. According to figure 24 in the datasheet I have to use a 150 uH inductor. Then I used the WEBENCH design tool and the inductor value is 680uH (see attached file).
Wich one should I use? Am I doing something wrong with the WEBENCH design tool ?
Thanks!