This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65123 fault detectoion threshold

Other Parts Discussed in Thread: TPS65120

In the datasheet on page 16 is mentioned:

All TPS6512x outputs are protected against a short circuit to ground. During steady-state operation, if the output

VMAIN, VGH or VGL falls below its fault detection threshold the device simultaneously turns off all three outputs.

Once VMAIN comes down to 700 mV typ, the GATE output is pulled to VIN, the auxiliary LDO (TPS65120/1/2) is

disabled and the device enters a shutdown state.

The auxiliary LDO present in TPS65120/1/2 has an integrated current foldback circuit for reliable short-circuit

protection.

The device can be enabled again by toggling the enable pins (RUN, EN) below 0.4 V or by cycling the input

voltage below the UVLO falling threshold (2.15 V typ).

But we cannot find what the value of this fault detection threshold  is.

Can you give this value to me?