Hello,
LM3431 has calculation tool of Mathcad.
Unfortunately , I don't have mathcad...
Thus, I tried simulation by webench.
But I can't get simulation result by below conditions.....
Could I have the result of mathcad by below conditions ?
If you need more information, please let me know.
---
Vin: 8.5V ~ 15.5V
Iout: 30mA/ch x 3 strings = 90mA
LED: 8series, 3 strings, Vf=3.6V(max)
Fsw : 200kHz
dimming frequency: 1.95kHz
dimming duty : 0.15% ~100%
---
Best Regards,
Ryuji Asaka