We have purchased a TPS61200EVM-179 evaluation board.
We measured the circuit's quiescent current at 2,7V input to be more than 100uA and it gets worse if we lower the value of Vin. It goes up to 250uA at 1,3 Vi input. EXCESSIVE! It is far from the published values of 50uA typ. and 70uA max. AT 1,2V
Is there a problem with that eval board? Is the IC really (normally) drawing that much quiescent current? It would make the TPS61201 unusable in our application,
Please help