Other Parts Discussed in Thread: UCD9222
Hi,
In the UCD9222 datasheet, Table 1 says to pull pin 20 (PM_Bus_Control) to 3.3V with a 10k ohm resistor. However, in the evaluation board design, it is pull low with 1M ohm resistor. Which one is corect?
Also, I am using it to run 320C6678 multicore DSP. Channel 1 is used to create variable power (0.9V-1.1V controled by VID bits from the DSP) and channel 2 makes fixed 1.0V. Does anybody have a configuration file to achieve this and is willing to share it? I appreciate help very much.
Thnak you.
Gasha Gataric