Hello,
The TPS2061/2/3/5/6/7 devices are rated at 1A continuous current with a current limit of 1.9A. I am wondering for the two and three channel devices if this applies for each channel. Can each channel provide 1A continuous?
Thanks,
Gui
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The TPS2061/2/3/5/6/7 devices are rated at 1A continuous current with a current limit of 1.9A. I am wondering for the two and three channel devices if this applies for each channel. Can each channel provide 1A continuous?
Thanks,
Gui
Gui,
Sorry for late reply, for TPS206x products, 1A continous current limit, Ios spec is 1.1A min, 1.5A typ, 1.9A max.
For multi channels, each channel is independent from each other, and same performance.
Can each channel provide 1A continious" Yes, each channel can provide 1A contnious.