Hello,
I want to use TPS51200 applying power as follows.
VIN=2.5V
VLDOIN=3.3V
According to the datasheet P1 FEATURES, explain “VLDOIN Voltage Range: 1.1 V to 3.5 V”
but TPS51200EVM User’s Guide Table 1(P3) explain “VLDOIN Voltage range (VLDOIN): 1.2V to 2.5V”.
http://www.ti.com/lit/ug/sluu323/sluu323.pdf
Q1:
Please advice which is correct recommended VLDOIN range.
Q2:
And also advice if there is any restriction between VIN voltage and VINLDO voltage(for example VIN > VLDOIN).
Best Regards.