Other Parts Discussed in Thread: LM20136
The LM20136 has two ways of calculating/estimating values for the external components for the device, using the design spreadsheet and webench. I have used both and there is a discrepancy between recommended inductance. Webench shows 2.2uH and the spreadheet shows 1.52uH. Also compensation values are different when I use the same values from webench in the design spreadsheet.
Here are the specifications:
- Vin: 4.5 to 5.25
- Iout =5.6A
- Vout = 3.3V
- Temp = 85C
- Soft-Start Time = 7ms
- Switching frequency = 410Khz (GND SYNC pin)
- inductor value -> 2.2uH, ESR -> 10.52mOhm
Which method is recommended for this case? And do you know where the discrepancy is coming from?
Thanks