Hi
please find the circuit below, BQ2004H used as Linear mode charge controller and settings are as follows
a) Charge rate : C/8
b)Termination: -ΔV method and C/8
c) Auto discharge and Temperature termination are not using.
BATTERY: NiMH pack (10 cells), 12V 1600mAh.
With these combinations, battery is charging for only 30 minutes . If i switch off the charge controller and switch ON again it will start charging and it will end for 20-30 minutes. Battery never reached full charge.
Please suggest me what will be the reason the battery is not reaching to full capacity.