Hi everyone,
I have built a buck converter using TPS53015. Input voltage is 24 Vdc, output voltage is set to 5 Vdc and desired maximum output current is 15 A. However, the efficiency of the built system is approximately 77 % at full load. Obviously, it is very low and this number comes with serious heating problem as I use both passive and active cooling for the manufactured PCB.
When I look at the TPS4530015EVM-126; input :8-22V output : 1.05 V and output current: up to 8 A. In the user's guide, the efficiency plot is given for different conditions and it is seen that the efficiency of the board is between approximately 84% -78% at maxiumum load. After that observation,I started to think TPS53015 is not suitable for my operating point. Moreover ,it is stated that typical applications of TPS53015 is POL regualiton in Low-Power systems. Since Low-Power systems is not quantitativewhat do I understad from this phrase? Can you give some quantitative explanation for Low-Power systems?
TPS53015 utilizes DCAP2 control method and in this method ripple injection is provided IC itself. From below document, it can be seen that ripple injection circuit consists of a Time Constant bloack and compression block. Since I am not able to get experimental data plot of Bode-Plot, can I learn the Time-Constant of the TPS53015? http://www.ti.com/lit/an/slva546/slva546.pdf
I appreciate with your help.
Regards,
Taha AKYOL