Hi,
I've got a ASUS Eee PC 701SD laptop with an original battery pack that uses BQ27210 for management. Original cells had died and, being a guy with a DIY spirit, I decided to try to replace them with new cells. The battery is now working but showing a symptom described below.
The battery appears to recharge fine. Once fully recharged, I'm getting a 'battery remaining' reading in Windows XP that seems correct judging by the manufacturer specs for a new battery. However, once the remaining battery capacity has steadily gone down from 100% to approximately 44%, the reading then immediately jumps to 7%. From there, it'll again decrease steadily to 0%. I can tell the big jump Windows reports is not based on the real battery performance, because the laptop will remain powered on for a long period of time at 0% reading (probably what power a 44% full battery is still able deliver)
I suppose the three possible reasons for this are
1. Some register value(s) associated with performance of the original cells being remembered by the management chip BQ27210. This results in a wrong capacity reading delivered to the laptop system.
2. Some other problem in the battery management circuit or laptop hardware.
3. Windows XP misinterpreting the data sent by the battery.
Unfortunately I don't have access to a new factory-made battery module that I could exclude/confirm the third option with. At some point, I might try booting from a Linux live CD to get a second OS opinion on the reading.
If anyone with experience in BQ27210 or a similar battery symptom has ideas, I'd love to hear them.