I have a UCC28600 based SMPS which is capable of delivering 5V@ 0.2Amp and 7.5V@0.15Amp but with my load ( an electronic board built around ARM processor LM3S815 requiring 120mA at full load) connected to it the output voltage is not stabilized at it's steady state values. So i just increased the soft start capacitor from 100nF to 10uF. with this high value of capacitor, supply is providing proper output with a delay of 3-4 seconds but it is getting stabilized with load connected to it.
Can we use this much capacitor on soft start pin.
Plz clarify.
rgds