Hi
Since coilcraft CT's are difiicult to get i was wondering if these from Pulse would do the job:
http://www.mouser.com/ds/2/336/-13316.pdf
of from farnell (Wurth ):
Another question, could i put the current transformer in the Source leg of the mosfet's ?
This would give less problems with capacitance between primary and secondairy . (large dv/dt)
(in this case it would also measure Ig )
Or can i put them on the cold side of the boost inductor ?
Some hints are welcome (PFC is targeted for 300W )
This my first PFC design.