Hello,
I am designing a power supply in which I need more than 6.5A current whereas as per Datasheet LM2677 provides 5A max. So, I was wondering if is it possible to parallel outputs of LM2677. Usually, I understand that it is not recommended to parallel two PSUs but LM2677 has Output Sync pulse so I though if we could give same oscillator pulse to both LM2677 and that way we could parallel two outputs without one output getting sinked in other.
Best Regards.