Hi,All
How much is range of input voltage about LM2991?
I checked LM2991 datasheet,but nothing about it.
I think that input voltage range is -3V to 24V,correct?
Best Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,All
How much is range of input voltage about LM2991?
I checked LM2991 datasheet,but nothing about it.
I think that input voltage range is -3V to 24V,correct?
Best Regards.
LM2991 Negative Low Dropout Adjustable Regulator
Depends on what the output voltage is programmed to.
Normal definintion for the LM2991 Operating Input Voltage would be :
(Vout − 1V) to (−26V)
The full operating voltage range may not be available if the load current is elevated, or package thermal resistance is elevated. Unfortunately, the datasheet does not go into thermal disspation in any detail, only the brief 'Note 4' under the Absolute Maximum ratings table.
Hi,Mr. Jones
Thanks you for quick reply!!
If there is another opportunity,please offer your support again.
Best regards!!