Hi,
I have designed a small piggyback card using TPS84250 for generating the 12.5V@1A from 16-36V DC input. The board was assembled and tested and able to see the 12.5V coming. But when I connect the o/p to a load which is a oscillator (OCXO@500mA), I am seeing the voltage getting dropped to 8.5V, some times I see the voltage fluctuation b/w 8.5V to 7V at very low frequency 10-16Hz . Please let me know what could be reason for problem.
I am attaching the schematic and layout for reference and below are the experiments which I had done already and no improvements found.
1) changed the RT resistor to 200 KOhms.
2) changed the soft start cap to 100nf.
3) added 20 ohms series resistor on the positive lines and found 9.5 volts at the IC end and 8.5 volts at the load end (OCXO). The OCXO is Expected to take < 500mA current
8311.SBCU_PSDB_PIGY_BACK_CARD.brd
Regards
Dharmendra G