Dear sir
Why does Rthj-a always bigger then Rthj-c?
Is there a figure indicated specifically?
And I try use CSD18501Q5A in the load condition as follow
VDS:20V
Vgs: 7V
Peak Id: 100A/0.001s
Continue Id: 30A/10s
Working Temperature:25°C
I do the working cycle that is on 10s off 5s
After 2 cycles, the CSD18501Q5A has rise up to 100°C
My target is 110°C after 30 cycles
Is this device unsuitable?