I have there modules that I want to inhibit at the same time. I have two PTH08080W and one PTH080260. Can I connect the Inhibit pins together and control with one FET?
Thank you,
Jose
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Joe:
The PTH08000W must have a dedicated inhibit pin control FET for each module.
The inhibit pins must not be connected together. The PTH modules have their own internal pull-up. Do not place an external pull-up to this pin.
Tom
Tom,
Thanks for the quick response. I don't have an external pull-up on any of the modules. All modules are power by the same source and I have one FET controlling the Inhibit on one of the supplies. Since they are all powered by the same supply, I thought I could use the same FET output to all three of my modules. My board is very tight so the would really save me.
Jose
Thanks for the response.
The PTH08080W and PTH08000 require a separate inhibit , open drain FET control for each module.
There are some proection features, OCP over temperature protection which can be overstessed when using common connection , inhibit FET, for more than 1 unit.
Regards
tom