Hello, I am trying to design a DCDC module which employs LMR61428. As I reading the datasheet:
" However if the VOUT is outside this range, the VDD pin should be connected to a voltage source whose range is between 2.5V and 5V. This can be the input voltage (VIN),"
Can I just tie VDD down to the battery? How about the boot and freq pins? Could you show me a schematic that will work for 12V output? Thank you.