Hi,
I've got an intermittent problem that I am trying to track down.
I am using the TPS22945 to protect a CPLD in the event of a latch up condition, but on occasion the TPS22945 will shutdown. I am monitoring the OC pin and it is constantly held low.
I've run some experiments with the over-current protection and the device works as expected - it shuts down for a period of time, then starts again. Similarly, it works as expected with the under-voltage lockout; once the input voltage rises above approx 1.4V the device enables and OC floats.
I believe the issue is caused by switching a load down stream that causes ground-bounce and causes the TPS22945 to enter its under-voltage lockout mode... however on occasion the device never restarts until a full power cycle is forced.
Has anyone seen anything similar, or can offer any advice?
Thanks